Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

EngineerZone
EngineerZone
ADIsimPE Library
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADIsimPE Library
  • Power Management
ADIsimPE Library
Documents problem simulating AD736 in ADIsimPE
  • Members
  • Tags
  • Cancel
  • Documents
  • 2015080- Anveshan 2014
  • AD539 Spice model
  • AD633 noise SImetrix model doesn't match datasheet
  • AD633 using ADIsimPE
  • AD8000 model
  • AD8227 does not work well on LTSpice
  • AD8336 spice model is not working
  • AD8336 with ADISimPE
  • AD8338 in PSPice
  • ADA2200 Encrypted Model
  • ADA2200 Spice Model
  • ADA4941-1 .cir
  • ADIsimPE 8.0 does not install - install shield stops at 20% and then does not respond.
  • ADIsimPE Design Tool model for ADP3050
  • ADIsimPE fails to update
  • ADIsimPE Full license version
  • ADIsimPE How do I check the number of node
  • ADIsimPE How do I define the correct symbol?
  • ADIsimPE How to use diffrential amp?
  • ADIsimPE License Issues
  • ADIsimPE Sallen key low pass filter Bode plot
  • ADIsimPE schematic from UG-241
  • ADIsimPE support Community
  • ADP2384 Design Tool vs ADISimPE results
  • ADP7142 Spice Model
  • ADP7183 Adjustable Voltage
  • AMP Noise Analysis
  • An error message appeared and said " *** ERROR *** The circuit is too large to simulate with this version. Too many analog nodes" .
  • Analogous mechaniocal electrical system- LTSPICE
  • Announcing the release of ADIsimPE 8.0
  • Bode plot in SimPE
  • Can an isolated DC/DC converter be created in ADIsimPower?
  • Can I import PSPICE models into ADIsimPE?
  • can not open model
  • Can you provide the non-linear model for HMC441LM1 power amplifier. I noticed that it is available in ADISimRF, but I wanted to incorporate it in my ADS simulations.
  • Can't find Comparator AD790 in ADIsimPE Library
  • Can't update ADIsimPE...?
  • CN0337 in ADIsimPE
  • Components not found in the new 7.20 ADIsimPE version
  • Could I have AD8250 model file?
  • Creating Spice model from time-domain oscilloscope data
  • DDS driven PLL ADIsimpll
  • different result's between ADIsimPE and Diff Amp Calculator!!!
  • encrypted models for amplifiers
  • Encrypted SPICE AD797 and AD734
  • excel 2007 crashing
  • high speed pulses with AD8009an in ADIsimPE
  • HMC477 and HMC733 library
  • HMC807 EVB schematic bug
  • How can to fix netlist after changing symbol pin order?
  • How do i link the Anlog Devices supplied AD630.cir file into my schematic/simulation using ADIsimPE
  • how to add LT6011 spice model to ADIsimPE?
  • How to add part to the library folder of ADIsimPE simulator?
  • How to avoid erasing old curves
  • How to emulate T/I design bench?
  • How to export ASCII text of simulated curve
  • How to simulate PD signal?
  • How to simulate signal?
  • How to use ADIsimPower with ADisimPE integration
  • I need to get 5V DC from an analogue telephone line without looping the line.
  • I replaced a single opamp with a ADA4700. This resulted in an*** ERROR *** The circuit is too large to simulate with this version. Too many analog nodes. Why?
  • I want to simulate with AD9833. For that i need SPICE model (library file) of AD9833. So please let me know where do I get it or is there any simulation software for that?. Thank you
  • I want to simulate with ADR3540.
  • In trouble simulating IN-AMP
  • Installed ADIsimPI right now and at first start it says that it only have 14 days remaining
  • Is it possible to simulate a battery in ADIsimPE?
  • Is there a license expiration period for ADIsimPE ???
  • Is there a LT3032 model available for ADIsimPE ?
  • Is there a way to integrate and simulate ADP5090 Model(SIMPLIS) and AD8210(SiMetrix) into a single circuit?
  • Is there a way to simulate the ADuM2250 in ADIsimPE ? It only appears to have an IBIS model.
  • Is there any difference between ADIsimPE and Pspice model?
  • Is there any way to fully simulate the ADP5054 with Buck 1 and Buck 2 in parallel?
  • Linear regulator models?
  • looking for some photo diode model
  • NEW DSP
  • Noise analysis
  • Noise analysis ADIsimPE
  • Noise analysis of ADIsimPE
  • Phase angle measurement
  • problem simulating AD736 in ADIsimPE
  • Program expired
  • PSpice model
  • Quick Start user Guide - UG706
  • Regarding ADP5301
  • Simulate with an AMP03, Importing Models
  • Simulation using AD8336, AD736 and AD8551 spice models in Pspice
  • Solution for ADIsimPE Update Error
  • Too many analog nodes in ADISIMPE Simulation
  • troubles with SPICE models of AD8033 and AD8065
  • Use LTspice .sub model in ADIsimPE
  • waht analog devices equpment i can apply for design capacitive humidity sensor with 0..10V analog output signal
  • What is ADIsimPE?
  • When I run efficiency on simulator...
  • Where can I post LTSpice questions?
  • Where do I find an ADIsimPE tutorial

problem simulating AD736 in ADIsimPE

Original Question: problem simulating AD736 in ADIsimPE by suryadeopa

simulating AD736.

I was trying to simulate AD736 rms to DC converter for 200mV input for fastest settling time. I have attached the circuit below. I might have made mistakes in selecting the Cav and Cf capacitors. 

When the input was a 1k sine wave the circuit was working properly. But when i increased the input frequency to 4k , the output started oscillating between +- Vcc. At first it seemed the output was settling to the correct rms value but then it started oscillating. I increased the input frequency to 32k, the oscillation started happening even earlier.

I am not able to understand why this is happening. Is it due to the capacitor values?

The requirements of my circuit is to find the rms value of a 32.786 kHz sine wave as fast as possible.

i have used ADIsimPE SIMetrix

the red curve is for 1kHz wave ,green is for 4kHz wave

thanks in advance

2806.attachments.zip

Verified Answer: RE: problem simulating AD736 in ADIsimPE by jstaley

Hello,

Thank you for your question. I would try the following:

1. Place a 10uF capacitor between CC and ground or between VIN and the signal source. Do not connect both to ground or else the circuit will never settle. It is like connecting both inputs of an op-amp to ground.

2. Place 10uF by-pass capacitors on the supply pins. A SPICE model never actually simulates a real component, especially an integrated circuit. A Spice model is a solution to a network large or small, but this is a mathematical construct, not real parts. You do get a solution very fast of course, but it's just a solution to a very large equation in most instances. If you want to learn how the part works get in touch with your local ADI contact and ask for an eval board. They'll probably give you one, anyway they're supposed to.  .

3. I like to add units to plot axes, it helps you if you have to lay the plot aside and you have to come back to it later.

Best,

js

  • Share
  • History
  • More
  • Cancel
Related
Recommended