Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
ADIsimPE Library
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADIsimPE Library
  • Power Management
ADIsimPE Library
Documents 2015080- Anveshan 2014
  • Members
  • Tags
  • Cancel
  • Documents
  • 2015080- Anveshan 2014
  • AD539 Spice model
  • AD633 noise SImetrix model doesn't match datasheet
  • AD633 using ADIsimPE
  • AD8000 model
  • AD8227 does not work well on LTSpice
  • AD8336 spice model is not working
  • AD8336 with ADISimPE
  • AD8338 in PSPice
  • ADA2200 Encrypted Model
  • ADA2200 Spice Model
  • ADA4941-1 .cir
  • ADIsimPE 8.0 does not install - install shield stops at 20% and then does not respond.
  • ADIsimPE Design Tool model for ADP3050
  • ADIsimPE fails to update
  • ADIsimPE Full license version
  • ADIsimPE How do I check the number of node
  • ADIsimPE How do I define the correct symbol?
  • ADIsimPE How to use diffrential amp?
  • ADIsimPE License Issues
  • ADIsimPE Sallen key low pass filter Bode plot
  • ADIsimPE schematic from UG-241
  • ADIsimPE support Community
  • ADP2384 Design Tool vs ADISimPE results
  • ADP7142 Spice Model
  • ADP7183 Adjustable Voltage
  • AMP Noise Analysis
  • An error message appeared and said " *** ERROR *** The circuit is too large to simulate with this version. Too many analog nodes" .
  • Analogous mechaniocal electrical system- LTSPICE
  • Announcing the release of ADIsimPE 8.0
  • Bode plot in SimPE
  • Can an isolated DC/DC converter be created in ADIsimPower?
  • Can I import PSPICE models into ADIsimPE?
  • can not open model
  • Can you provide the non-linear model for HMC441LM1 power amplifier. I noticed that it is available in ADISimRF, but I wanted to incorporate it in my ADS simulations.
  • Can't find Comparator AD790 in ADIsimPE Library
  • Can't update ADIsimPE...?
  • CN0337 in ADIsimPE
  • Components not found in the new 7.20 ADIsimPE version
  • Could I have AD8250 model file?
  • Creating Spice model from time-domain oscilloscope data
  • DDS driven PLL ADIsimpll
  • different result's between ADIsimPE and Diff Amp Calculator!!!
  • encrypted models for amplifiers
  • Encrypted SPICE AD797 and AD734
  • excel 2007 crashing
  • high speed pulses with AD8009an in ADIsimPE
  • HMC477 and HMC733 library
  • HMC807 EVB schematic bug
  • How can to fix netlist after changing symbol pin order?
  • How do i link the Anlog Devices supplied AD630.cir file into my schematic/simulation using ADIsimPE
  • how to add LT6011 spice model to ADIsimPE?
  • How to add part to the library folder of ADIsimPE simulator?
  • How to avoid erasing old curves
  • How to emulate T/I design bench?
  • How to export ASCII text of simulated curve
  • How to simulate PD signal?
  • How to simulate signal?
  • How to use ADIsimPower with ADisimPE integration
  • I need to get 5V DC from an analogue telephone line without looping the line.
  • I replaced a single opamp with a ADA4700. This resulted in an*** ERROR *** The circuit is too large to simulate with this version. Too many analog nodes. Why?
  • I want to simulate with AD9833. For that i need SPICE model (library file) of AD9833. So please let me know where do I get it or is there any simulation software for that?. Thank you
  • I want to simulate with ADR3540.
  • In trouble simulating IN-AMP
  • Installed ADIsimPI right now and at first start it says that it only have 14 days remaining
  • Is it possible to simulate a battery in ADIsimPE?
  • Is there a license expiration period for ADIsimPE ???
  • Is there a LT3032 model available for ADIsimPE ?
  • Is there a way to integrate and simulate ADP5090 Model(SIMPLIS) and AD8210(SiMetrix) into a single circuit?
  • Is there a way to simulate the ADuM2250 in ADIsimPE ? It only appears to have an IBIS model.
  • Is there any difference between ADIsimPE and Pspice model?
  • Is there any way to fully simulate the ADP5054 with Buck 1 and Buck 2 in parallel?
  • Linear regulator models?
  • looking for some photo diode model
  • NEW DSP
  • Noise analysis
  • Noise analysis ADIsimPE
  • Noise analysis of ADIsimPE
  • Phase angle measurement
  • problem simulating AD736 in ADIsimPE
  • Program expired
  • PSpice model
  • Quick Start user Guide - UG706
  • Regarding ADP5301
  • Simulate with an AMP03, Importing Models
  • Simulation using AD8336, AD736 and AD8551 spice models in Pspice
  • Solution for ADIsimPE Update Error
  • Too many analog nodes in ADISIMPE Simulation
  • troubles with SPICE models of AD8033 and AD8065
  • Use LTspice .sub model in ADIsimPE
  • waht analog devices equpment i can apply for design capacitive humidity sensor with 0..10V analog output signal
  • What is ADIsimPE?
  • When I run efficiency on simulator...
  • Where can I post LTSpice questions?
  • Where do I find an ADIsimPE tutorial

2015080- Anveshan 2014

Original Question: 2015080- Anveshan 2014 by KoushiK_KopS

I m trying to simulate this circuit in ADIsimPE. But i m getting the following error.

"*** ERROR *** Cannot find DC operating point - No convergence in pseudo transient analysis"

what does this error mean and how to debug it?.


Verified Answer: RE: 2015080- Anveshan 2014 by JGunao

Hi Koushik,

Transient analysis' convergence error in ADIsimPE commonly occurs when there are circuit problems that exist in which the simulator itself can't handle. In your case, the most probable reason that the error occured because the pin order of the AD8221 model is incorrect.

We are currently working on this, so that it will be fixed in the next version of ADIsimPE.

As of now, the solution to this problem is to change the pin order of the AD8221 model using the Edit Symbol command. To do this, please right click to the AD8221 symbol and click Edit Symbol. When the symbol window comes up, under the "Property/Pin" choose "Edit Pin Order". Pin order must be re-arranged like this.

Click OK, then under "File" click "Save" then "OK". Close the symbol window. After this, re-run your simulation. You can now expect your simulation to run without any error.

On the other hand, I also noticed that your input is not properly grounded. Kindly add a ground symbol to the input side, otherwise you'll not get the desired output.

I hope this helps.

Regards,

Jay


Question: RE: 2015080- Anveshan 2014 by JGunao

Hi Koushik,

I'm glad that I helped you in your simulation. Please let me know if you need anything else. Also, thanks for using ADIsimPE.

Regards,

Jay


Question: RE: 2015080- Anveshan 2014 by KoushiK_KopS

Thanks a lot JGunao.

its working properly now.

  • Share
  • History
  • More
  • Cancel
Related
Recommended