Post Go back to editing

ADP7183 Adjustable Voltage

I am using the ADP7183 in adjustable mode to achieve the DC voltage of -0.9V.

Following the formular in the datasheet, the output voltage is given as V=-0.5(1+R1/R2).

We set R1=8k Ohms and R2=10k Ohms.  Under such a setting, the adjustable output voltage is supposed to give V=-0.9 V.

However, in our test, we measured the output voltage as V=-1.5V in such a setting.

.  
We also measured the voltage at the Low noise reference voltage pad VA is -0.9 V. 


We tried all possible ways to obtain the -0.9V in this way but still it is not successful. 

Strangely, we have another ADP7183 using a similar setting but only replacing R1=4k. It ouputs R=-0.5(1+R1/R2)-0.5(1+4k/10k)=-0.7V.


We are very grateful if you could help any suggeustions what is the cause of the problem.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.