Article What is the PGOOD output maximum sink current of MAX20410?

When PGOOD is asserted low, the max current sink advisable is 1 to 2 mA, maximum of 3 mA.  Anything above 2mA will be considered outside nominal application and should be tested.