Q: What is the MAX20098 VLIMIT accuracy for VOUT<2.5V?
A: The VLIMT accuracy could reduce if VOUT<2.5V. It is expected that the VLIMIT accuracy will not exceed 15% variation, which gives a range of 60mV (min), 80mV (typ), 102mV (max).
MAX20098
Production
The MAX20098 is an automotive 2.2MHz synchronous step-down controller IC with 3.5µA IQ. This IC operates with an input-voltage supply from 3.5V to 42V...
Datasheet
MAX20098 on Analog.com
Q: What is the MAX20098 VLIMIT accuracy for VOUT<2.5V?
A: The VLIMT accuracy could reduce if VOUT<2.5V. It is expected that the VLIMIT accuracy will not exceed 15% variation, which gives a range of 60mV (min), 80mV (typ), 102mV (max).