Article When output voltage of MAX5082 is 5V, how to set the voltage divider resistance? In addition, what is the output voltage of the "LX" pin?

As shown in Figure 5 in the datasheet, the output voltage is 3.3V

According to the calculation formula of Page11, if an output voltage of 5V is required, R3=6.81Kohm and R4=2.2Kohm.

In addition, when the chip is working, a square wave switching waveform can be measured from the "LX" pin.