Article In 2 +2 configuration what will be the Default output voltage if M1_VOUT=0.72V is not equal M2_VOUT=1.495V?

In a phase combined configuration, only the master phase registers are active. The slave phase registers are ignored. In a 2+2 configuration, M2_VOUT and M4_VOUT  are ignored, and the rail1 (Phase 1+ Phase 2) and rail 2 (Phase 3 + Phase 4) outputs are set respectively by M1_VOUT and M3_VOUT registers.