Article When testing a 5V@6A isolated power supply designed with the MAX17599 power IC, we found that during power-on, the output voltage rise time was only 200-300us. Such a short rise time can cause the load to go into lockout. We hope that you can provide a sol

As shown in the figure below, in the feedback circuit, the value of resistor R17 from pin 3 of the photocoupler to ground will affect the rise time of the output voltage; The larger the resistance, the longer the output voltage rise time. If the resistor is changed to 470 ohms, the output voltage rise time becomes approximately 3ms.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.