Article What are the features in MAXIM nano-power boost solution to realize low power consumption?

 
1. Low quiescent current. Our quiescent current is as low as 300nA
 
2. True Shutdown Mode. When our device is disabled, the output is disconnected from the input and is 0V instead of a voltage that is lower relative to the input.
 
3. Unique sampling method for output voltage selection: Using RSEL eliminates wasting current continuously through feedback resistors.