Article Is it possible to add an external load to the VCC pin of MAX17504?

It is acceptable to have a small external load on the VCC pin. For example the EVKIT for this IC uses a 10kOhm resistor on the VCC pin to act as a pullup for the /RESET pin which results in a ~0.5mA draw. 

The VCC pin supplies the gate drivers within the IC so it is critical for proper operation that this pin is not loaded externally above 1mA.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.