Otherwise, the parts are the same. Note that this is different nomenclature from other Maxim products - usually power modules have "MAXM" in the name and the discrete step-down converter/controller IC in the module has "MAX" in the name.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX17515
Last Time Buy
The MAX17515 is a fixed-frequency, step-down power module in a thermally efficient system-in-package (SiP) package that operates from a 2.4V to 5.5V input...
Datasheet
MAX17515 on Analog.com
MAXM17515
Last Time Buy
The MAXM17515 is a fixed-frequency, step-down power
module in a thermally-efficient system-in-package (SiP)
package that operates from a 2.4V to 5.5V input...
Datasheet
MAXM17515 on Analog.com