A MAX8881EUT18-T that has the output set to 1.8V was tested in the lab. At 2.5V Vin, the current limit is at 220mA which is above the minimum specification for current limit.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX8881
Production
The MAX8880/MAX8881 are ultra-low supply current,
low-dropout linear regulators, capable of delivering up
to 200mA. They are designed for battery-powered...
Datasheet
MAX8881 on Analog.com