Article ADP2504 Issues with supplied current and current limiting

Question

The ADP2504 not achieving the max 1 amp as defined in the spec.

Answer

The ADP2504 is designed to start-up with a maximum of 100uF, if you have
additional capacitance besides the 22uF shown on the datasheet schematics that
may result in the output voltage stuck at 80% of 5V because of the current
limit.