Question
what is the max power input frequency for the ADP1048
(more than 60Hz ?). I need 500Hz - is this possible?
Answer
yes - the ADP1048 kann also be used from 500Hz - 1kHz (e.g. net in an airplane)
ADP1048
Recommended for New Designs
The ADP1047 / ADP1048 are digital power factor correction (PFC) controllers that provide accurate input power metering capability and inrush current...
Datasheet
ADP1048 on Analog.com
Question
what is the max power input frequency for the ADP1048
(more than 60Hz ?). I need 500Hz - is this possible?
Answer
yes - the ADP1048 kann also be used from 500Hz - 1kHz (e.g. net in an airplane)