Article In MAX16046, one of the GPIO is configured as “Any Fault” output. Under what conditions, does this “Any Fault” output gets asserted?

In MAX16046, different voltage thresholds such as Undervoltage, Overvoltage or Early-Warning are set for each monitoring channel. If the monitoring channel’s input voltage violates any of the above mentioned thresholds, then a fault condition occurs. Any GPIO configured as “Any fault” output is an “Active Low” output. As soon as the monitoring channel’s voltage violates any of the respective threshold, “Any fault” output becomes LOW irrespective of any other register setting in the chip. Whenever monitoring channel’s voltage comes within the specified thresholds, “Any Fault” output gets de-asserted and becomes High.