As per Typical Operating Curve we can use CSWT capacitor to a value up to 0.1uF which can set Extended watchdog timeout to approx. 65s.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX6746
Production
The MAX6746–MAX6753 low-power microprocessor (µP) supervisory circuits monitor single/dual system supply voltages from 1.575V to 5V and provide maximum...
Datasheet
MAX6746 on Analog.com
As per Typical Operating Curve we can use CSWT capacitor to a value up to 0.1uF which can set Extended watchdog timeout to approx. 65s.