Article Can the CS1 pin of the ADP1043A, ADP1046A, ADP1050, ADP1051, ADP1055 be floating?

The CS1 pin of the ADP1043A, ADP1046A, ADP1050, ADP1051, ADP1055 can not be floating (no resistor is connected between the CS1 pin and ground). there is a tiny source current in this pin. If CS1 pin is floating, the voltage of CS1 pin will be higher than 1.2V which will trigger the cycle-by-cycle limiting and disable some or all PWM outputs..