The two pins in middle of the package are POK and FPWM:
POK is open drain, yes, you can keep it float if not used.
FPWM has a ~800kohm pull down resistor, float will set the part in auto skip mode.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX77827
Production
The MAX77827 is a high-efficiency buck-boost regulator targeted for one-cell Li-ion powered applications with the lowest typical quiescent current in the...
Datasheet
MAX77827 on Analog.com
The two pins in middle of the package are POK and FPWM:
POK is open drain, yes, you can keep it float if not used.
FPWM has a ~800kohm pull down resistor, float will set the part in auto skip mode.