Article What is the required power rating of the 4.7Ω resistor between VCC and DRV in the MAX16814 Typical Application Circuit?

The maximum output current of the Vcc regulator is 100mA, therefore for a 4.7Ω resistor the maximum power loss across would be 47mW. Any resistor with a power rating ~1.5 times greater than this value is acceptable.