In this EVKIT the transformer’s secondary winding is used directly to drive the synchronous secondary side mosfet. This topology is called self-driven. It is a simple technique, however, transformer leakage…
No. MAX5995B has automatic MPS function,. It needs setting the current via resistor on SL pin (connect across SL pin and GND). As for LED pin, it needs connect to GND to sink the current at least.
Not every PSE can support such lower duty cycle( 5% ). For better PSE compatibility, we provide different options by connecting a resistor (no worse than 1% accuracy) between AUC and VSS to program the…
Question: If I don’t have a resistor on the Rcls pin, the circuit still operates but I don’t know what Classification is presented to the PSE?
Answer: When the PSE detects a connected PD, it will send…
The high quiescent current is associated with the LED pin sourcing current to ground directly. When the LED pin is connected to ground, it can lead to higher than normal current draw. The pins nWK and…