Article MAXM17575 thermal conductivity junction to case

Question:
Do you have any information about the thermal conductivity Junction to Case of the MAXM17575?

On the datasheet I found only the thermal conductivity of  the MAXM17575 mounted on the demo board.

Power dissipation: 750mW
Maximum ambient temperature: 65°C



Answer:

We do not have this information since we do not expect customers to add thermal pads etc on top of the case- they will need to make their own measurements in this regard.
The modules are designed to sink heat into the board and deliver the intended output current.


 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.