The minimum reset threshold of the supervisory circuit, after taking into account of the maximum absolute error, should be higher than the minimum operating voltage of the microprocessor and the other…
There's a mismatch on pin name WDI.In the pin description on page 5 this pin name has over bar. But on page 9 it doesn't have an over bar. The WDI should not have any over bar. The pin description is wrong…
While there is no guarantee, many Maxim's supervisory products can maintain a valid, logic low reset output /RESET even when V CC is lower than the minimum working voltage. However, when V CC falls below…