No, the MAX77812 can be used for a maximum output voltage of 2.7V if you use a resistor divider on the output. It will however have highly derated maximum output current, even at 2.7V.
3.3V output voltage…
MAX77812 Buck1 and Buck2 share a common input (IN12) while Buck3 and Buck4 share a common input (IN34). Hence, I IN12 measures the total input currents of Buck1 and Buck2. To measure the input current…
Question:
Please advise MAX77812 Delay from CE=High to Top-level Bias Ready (Both VSYS and VIO must be within the operating ranges).
Answer:
15us (min) 50us(typ) 140us(max)
Question:
Please advise MAX77812 delay time from EN goes Hi to Vout rising point.
Answer:
If the debounce timer setting is 64us (default)
90us(min) 120us-160us (typ) 220us(max)
If…
Please advise MAX77812 Soft-start Slew-rate variation.
Answer:
The electrical characteristics table provides slew-rate typical values only. Although not tested or guaranteed, the product design team…
A blind via connects an outer layer to one or more inner layers in a printed circuit board. It does not go through the entire's board height. They are particularly used in designs where there are space…