Article MAX77643 efficiency issue

MAX77643's efficiency depends on the working mode.

For example, if Vin=3.7V, Vout=1.8V, we need set it to Buck mode, then the efficiency will be like below. If set to Buck-Boost mode as default, the efficiency will be less than 80%.

For Vin=3.7V, Vout=5.0V, we need set it to Boost mode, then the efficiency will be like below. If set to Buck-Boost mode as default, the efficiency will be less than 60%.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.