MAX77643AANA+: FAQ

MAX77643AANA+: FAQ
  • Created
Was this helpful?
  • MAX77643 efficiency issue

    MAX77643's efficiency depends on the working mode. For example, if Vin=3.7V, Vout=1.8V, we need set it to Buck mode, then the efficiency will be like below. If set to Buck-Boost mode as default, the…
  • MAX77643 fault issue

    When changing MAX77643 output from one low volt to high volt, sometimes it will trigger fault issue. When the output voltage is increased, it takes time to ramp up to the target voltage. During this…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.