Article In most cases, customer’s waveform input to MAX77501 does not start from 10V(wave trough) but from 50V(balance point). So if the input starts from 50V, will some POP noise heard or felt? Or some other issue?

If there is a sharp transition from 10V to 50V a ‘pop’ sound will occur on the piezo. This is why it is recommended that all haptic waveforms start at 10V. If the waveform has to start at 50V, it's recommended including a ramp to slow down the transition from 10V to 50V in the waveform file.