Article What is Valley Current Limit in the MAX77324?

The control scheme in this converter is a constant on-time control which sets the on-time to a fixed value while extending the off-time to reduce current below the limit. This valley current limit control senses the low-side switch current to keep the on-time constant and to extend the off-time, reducing current below this limit (1.1A).

The device features a robust overcurrent protection scheme that also protects the device and inductor under overload and output short-circuit conditions. A cycle-by-cycle peak current limit turns off the high-side MOSFET and turns on the low-side MOSFET whenever the high-side MOSFET current exceeds the internal peak current limit (3A). The low-side MOSFET remains on until the inductor current reduces to the valley current limit (1.1A). After that, the high-side MOSFET is turned on again and the cycle repeats.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.