MAX6895AALT+: FAQ

  • Created
Was this helpful?
  • MAX6895AALT+ Top Marking Dots

    Question: What are the 3 dots on the MAX6895AALT+ top mark and how do they affect pin 1 orientation? . . . + Pin 1 Pin 2 Pin 3 Answer: There is no significance to the three dots…
  • Maximum transient duration versus input overdrive in the MAX6895

    In microprocessor supervisors, Maxim specifies the amplitude and duration that a glitch on Vcc needs to have to trigger the reset circuitry. For the MAX6895, see the graph at the bottom left TOC in page…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.