MAX6735_KASYD3+_A1: FAQ

MAX6735_KASYD3+_A1: FAQ
  • Created
Was this helpful?
  • MAX6735 vs MAX6735A

    The A version is specified for -40°C to 125°C while the non A version is rated for -40°C to 85°C. In addition, the RSTIN input current specification for the A version is ±100nA over temperature (up…