MAX668EVKIT+: FAQ

MAX668EVKIT+: FAQ
  • Created
Was this helpful?
  • How do I change the MAX668EVKIT output to 5V@4A

    The original output voltage of the MAX668EVKIT is 12V@1A, if you want to change it to 5V@4V, you can change the following parameters: a. The input capacitor C1: 150uF 20%, 6.3V, X5R ceramic capacitor…