If the SRT pin of the MAX6412 is left open then the device is operated as a voltage detector with the standard Reset Timeout Period of 0.275ms. On power-up, the /RESET pin remains low until Vcc crosses…
The /RESET output will remain low until Vcc reaches its threshold. As soon as Vcc crosses its threshold, the /RESET output will remain low for the Reset Timeout Period as determined by the capacitance…
The datasheet electrical characteristics only has reset timeout period min and max values for a 1500 pF capacitor. But what if you want to know the min and max values for a different timeout period, say…