MAX5971BETI+: FAQ

MAX5971BETI+: FAQ
  • Created
Was this helpful?
  • Is there any MAX5971B Thermal Test Data available?

    Maxim did not run bench thermal tests on the MAX5971B and does not plan too in the future. However, the device's thermal behavior under EC-table Global Conditions can be addressed using the MAX5971B integrated…
  • MAX5971B Startup issues due to floating INT| pin

    Issue: A customer's 48V Power over Ethernet (PoE) Power Sourcing Equipment (PSE) required 2 channels, I2C communication and did not require an Interrupt signal. The dual channel PSE was implemented using…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.