Article When output voltage of MAX5082 is 5V, how to set the voltage divider resistance? In addition, what is the output voltage of the "LX" pin?

As shown in Figure 5 in the datasheet, the output voltage is 3.3V

According to the calculation formula of Page11, if an output voltage of 5V is required, R3=6.81Kohm and R4=2.2Kohm.

In addition, when the chip is working, a square wave switching waveform can be measured from the "LX" pin.


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.