Article Can the MAX40200 be connected in parallel to support 2A output current?

Due to variations between devices, there exist differences of the on-times and forward voltages between two diodes. When connected in parallel, if one diode conducts first, then all of the 2A current may flow through a single diode, thereby possibly causing damage.