Due to variations between devices, there exist differences of the on-times and forward voltages between two diodes. When connected in parallel, if one diode conducts first, then all of the 2A current may…
Can the MAX40200 handle continuous 1A current reliably?
This device is available in SOT23-5 and WLP packages. The WLP package can handle more current as compared to the SOT23-5. The absolute maximum…
Yes, the MAX40200 will be stable with an output capacitance greater than 100uF. The output does need at least 0.33uF, but there is no upper limit on the output capacitance. The datasheet lists the spec…