MAX38888ATD+T: FAQ

MAX38888ATD+T: FAQ
  • Created
Was this helpful?
  • Can MAX38888 boost to the voltage the same as VSYS input?

    Normally it can't. The normal boost output feedback pin FBS is set to 0.5V, but the threshold is 0.56V if we want MAX38888 to charge to the SuperCAP. So if the system conect 5V to the VSYS pin, and…
  • Does Maxim have a SuperCap backup regulator IC?

    The MAX38888 is a storage capacitor or capacitor bank backup regulator designed to efficiently transfer power between a storage element and a system supply rail in reversible buck and boost operations…
  • MAX38888 (Rev. 2; 10/18) Datasheet Corrections

    Correction of MAX38888 datasheet (Rev. 2; 10/18) errors in calculations for super capacitor voltage configuration: Page 9, under the section titled Super Capacitor Voltage Configuration , the…
  • Operation issue for MAX38888

    Q: When use MAX38888, found the SuperCap can not be full charged, it is around 2.4V. Removing the charge voltage, it can not be discharged. Even charge the SuperCap to full directly, it still can not discharge…
  • Why MAX38888 can not be charged with 5V but can be boost output to 5V?

    They will not be able to boost back to 5V because MAX38888 will require the supply to be above VSYS max (5V) to start charging. The device requires VSYS to be 12% above the boost target to start charging…