Input for Fan 3 should be provided from PWMOUT3 pin of MAX31790. Correct image is shown below.
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
MAX31790
Production
The MAX31790 controls the speeds of up to six fans using six independent PWM outputs. The desired fan speeds (or PWM duty cycles) are written through the...
Datasheet
MAX31790 on Analog.com
Input for Fan 3 should be provided from PWMOUT3 pin of MAX31790. Correct image is shown below.