Article How to avoid Fan_Fail to trigger for unused ports in the MAX31790?

We can use Fan Fault Mask  Registers (12h, 13h) to mask faults on selected fans from asserting the FAN_FAIL output.
Also in PWM mode you can set the target duty cycle of the unused fans as zero to mask the fan-failure detection of that fan.(see PWM Mode Failure Detection section on page 13 of datasheet). In RPM mode, fan failure detection is masked when the TACH Target Count register is set to full scale.

 

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.