Article Is there a way to force the maximum fan speed on the MAX31785 using a pin?

Configuring the FAULT pin as an input pin via the MFR_FAULT_RESPONSE(register 0xD9) Bit0 = '1' will force the fan output to 100% duty cycle when the pin is externally asserted. Bit 0 of the MFR_FAULT_RESPONSE register must be set to a value of 1 for every page (channel) that the 100% duty cycle behavior is desired when the /FAULT pin is drive low. Since FAULT is an active-low, open drain input/output, the way to force the 100% duty cycle would be to tie FAULT to VDD via R_pullup and then pull it to ground to assert. 
 
 
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.