Article Is there an example that shows how to use SMBus/PMBus of the MAX31785? Can you describe how to use the Page command?

 
Page 0-22 (decimal) is used to select individual fan, temperature sensor, or remote voltage connected to the ADC. For control associated with each page, refer to Table 9 in the datasheet (Rev 3 8/12). Once selected, all control commands are for that page only.
 
To select a page, send slave address, followed by page command, and then the data (page number). For example, by sending Start condition--Slave address--Page command (0x00) --data (0x00), Page 0 is selected. Page 0 is associated with fan connnected to PWM 0. You can then use commands to configure the fan. For commands available for Page 0, refer to Table 1 of the datasheet. For example, 0x3A (FAN_CONFIG_1_2) command can configure the fan. If you wish to control other fans, use the Page command to select the fan, then use the control commands to configure it.
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.