Article When MAX25610 is used to drive 5 strings/15V LED application, the chip will shut down when the input voltage reaches about 20V. How can I solve it?

In buck-boost mode of MAX25610, the input OVP is Vin+Vled.    

So for MAX25610 whose OVP is around 33V, it is indeed turned off by entering OVP protection.

If you need to operate at 24V Vin and 5 LEDs in buck-boost, you need to use LED driver like MAX25612.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.