MAX20801TPBA+: FAQ

  • Created
Was this helpful?
  • MAX20801 Minimum Operating Voltage. 1.5V or 6.5V?

    The MAX20801 datasheet lists a minimum operating voltage of 1.5V, but the EC table lists 6.5V as the minimum Vin voltage. Which is correct? 1.5V is the minimum voltage at which the IC can work, but…
  • What is the output voltage of MAX20800/MAX20801?

    The output of MAX20800/MAX20801 depends upon the load or battery to which the IC is connected. For example if MAX20800 is connected to a 6V battery the output voltage of the converter will be 6V. MAX20800…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.