Article What is function of the thermistor in a MAX20361 system and can it be avoided?

There is a thermal monitoring feature in MAX20361 using an external thermistor which ensures that charging stops when the system gets too hot or too cold to save the battery. If we use MAX20360 PMIC along with MAX20361 then we can avoid the external thermistor in MAX20361 as this feature will be taken care of by the MAX20360 PMIC.