MAX20057ATIA/VY+T: FAQ

MAX20057ATIA/VY+T: FAQ
  • Created
Was this helpful?
  • What is the minimum operating voltage of MAX20057?

    The MAX20057 boost controller cannot start operation with input voltage less than 4.5V(typ). The initial input voltage should be at least 4.5V. However, once the converter starts it continue to work even…