Article What is the minimum external bias voltage that can be supplied to MAX17690 INTVCC pin?

Normal range of recommended external source voltage is between 8V and 16V.  However, the maximum external source voltage should be always higher than or equal to the minimum input voltage. This is to ensure that the body diode of the internal LDO does not conduct. (This diode exists from INTVCC to IN)