Article In the MAX17690EVKITA, why is a 62mOhm resistor used?

Although the calculated value is ~70mOhm, a 62mOhm resistor is used to ensure the circuit doesn't go into current limit before 1A.

The larger 70mOhm does not take into account noise spikes which could force the design into current limit too early. The 62mOhm chosen wil give the design enough tolerance to ensure it goes into current limit only above a 1A output.