The MAX17596 has a VIN range of 4.5V to 36V. In Flyback applications where the input DC voltage is higher than 36V we cannot use VDC as a direct input to the Vcc pin. Therefore, the required VIN is generated…
The flyback converter can be designed to operate either in continuous or discontinuous modes. In DCM, discontinuous conduction mode of operation, the transformer core completes its energy transfer during…
The main difference between the MAX17596 and the MAX17597 is the duty cycle. The MAX17596 has a maximum duty cycle of 50% while MAX17597 has a maximum duty cycle of 95%. Other than that there is no difference…