MAX17559_CJ+_A1: FAQ

  • Created
Was this helpful?
  • MAX17559 alpha Selection

    Q: On page 19 of the datasheet it is not clear how to select alpha (offset introduced at the Vout). Secondly if we select alpha=0.1% as said in the datasheet then the resultant R1 should be less than or…
  • MAX17559のPGOOD端子の電気的特性

    PGOODはオープンドレインの信号です。 この端子は5Vまでプルアップすることが出来ます。 この端子の絶対最大定格はデータシートの絶対最大定格にある通り、-0.3Vから+6Vです。 この端子のリーク電流は typ=0nA, Min= -100nA, Max= 100nAです 。 PGOOD のディレイは: 10us (アンダーボルテージ、オーバーボルテージ(立ち上がり、立下がり)時PGOOD最大シンク電流は…
  • Whats the main difference between the MAX17558 and the MAX17559?

    These two devices are exactly the same except that MAX17559 has a Soft-Stop feature which is not present in the MAX17558.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.