Typical Quiescent current at standard test condition is 118uA (+/- 35%) . And with temperature (-40C to +125C) it can change by +/- 25%. The maximum current can be 200uA.
When measuring small signals such as ripple voltage in a power supply circuit, the measurement loop must be minimized to avoid collecting noise from the environment. As shown in the figure below, connect…