Article External loop compensation of MAX17502

Question:  External loop compensation of MAX17502. The value of RZ calculated for the design in figure 9 of the datasheet comes out to 36kohm (6000 x 50000 x 10uF x 12V). But in the datasheet RZ=20kohm.  Kindly explain the discrepancy in calculations


Answer: Rz is indeed set according to the formula. However the value used for CSEL in the equation should be the actual value of that O/P capacitor when the voltage across the O/P capacitance is 12V (the capacitance value of a ceramic capacitor decreases with increasing voltage across it - this decrease can be established from the capacitor manufacturers datasheet)
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.